Conexant Offers High-Performance RF Components For Wireless Infrastructure Market
Gwen Carlson
Conexant Systems, Inc.
949-483-7363
gwen.carlson@conexant.com
Heather
McLaughlin
Benjamin Group/BSMG Worldwide
949-260-1300
heather_mclaughlin@benjamingroup.com
Conexant Offers High-Performance RF Components
For Wireless Infrastructure Market
Ultra Linear Power-Amplifier Drivers And Receiver
Front-End ICs
Are First Standard Products for Wireless Base Stations
NEWPORT BEACH, Calif., Mar. 19, 2001 — Conexant Systems, Inc. (NASDAQ: CNXT), a worldwide leader in semiconductor solutions for communications applications, today announced its first solutions in a new product portfolio of broad range high-performance radio frequency (RF) and microwave components for wireless infrastructure equipment. The new products are designed to meet the performance, functionality and cost requirements of current- and next-generation cellular base stations. Conexant's wireless infrastructure product portfolio includes the new CX42053 and CX42054 diversity downconverter/receiver front-ends designed for cellular/PCS base station receivers and new ultra linear Power Amplifier (PA) drivers (CX65001, CX65002 and CX65003) for cellular/PCs, and other wireless transceivers operating up to 2500 MHz.
"Next-generation wireless networks are placing greater demands on the base stations that transmit and receive signals in cellular and PCs systems," said Mohy Abdelgany, vice president, RF components and subsystems for Conexant. "To meet these demands, RF designers are continually challenged to increase base station transceiver performance and functionality, while reducing size, power consumption and overall system costs. Conexant is uniquely positioned to address these challenges with our comprehensive RF and mixed signal process and packaging portfolio, extensive circuit design libraries, and our proven track record in wireless component and system design."
Conexant's wireless infrastructure ICs combine superior performance and functionality in a low-cost solution. Target applications include base station transceivers used in global system for mobile communication (GSM), code division multiple access (CDMA), time division multiple access (TDMA), advanced mobile phone service (AMPS) network, and next-generation enhanced data for GSM (EDGE), General Packet Radio System GPRS, as well as 3G (UMTS, WCDMA), wireless LAN and wireless local loop networks.
Product Details
Among the first devices in the new product portfolio of high-performance, low-cost components are two diversity receivers/downconverters, CX42053 and CX42054, operating from 700 to 1000 MHz, and 1700 to 2500 MHz, respectively. These ICs may be used in single- or dual-channel configuration, with each channel featuring an LNA, Low Noise Amplifier, double balanced mixer, and LO (local oscillator) buffer amplifier. Both receivers are designed to meet the stringent requirements for high dynamic range, input third order intercept point (IIP3), and low noise in cellular/PCs base station receivers. Their highly integrated design provides a reduced cost solution and a convenient alternative to discrete components. Utilizing Conexant's GaAs metal semiconductor field effect transistor (MESFET) process, these receivers offer the ideal combination of outstanding performance, flexibility and functionality for base station receivers.
Based on Conexant's leading GaAs heterojunction bipolar transistor (HBT) technology, Conexant's new series of ultra linear PA drivers (CX65001, CX65002, CX65003) offer a typical P1dB of 23 to 25 dBm, at frequencies of 200-600 MHz, 7000-1000 MHz and 1400-2500 MHz, respectively. Typical output third order intercept point (OIP3) of 44 dBm and efficiency of 37 percent (CX65002) are among the highest in the industry at this price level. On-chip active bias, simple matching, superior performance and low cost, make them ideal for a variety of wireless applications - from mobile base stations to wireless LAN and telemetry amplifiers.
Conexant's broad range of high-performance RF and microwave components for the wireless infrastructure complements its broad portfolio of solutions for wireless handsets, which includes complete system solutions, RF subsystems and standalone components. Conexant's infrastructure component roadmap includes a planned rollout of LNAs, modulators, demodulators, down converters, linear PA modules and other components based on the company's leading process technologies.
Pricing And Availability
Conexant's PA drivers are priced starting at $5.19 each in quantities of 1,000. Conexant's receiver front-end ICs are priced starting at $15.55 each in quantities of 1,000 units. For availability, contact Avnet RF & Microwave in North America at 800-532-0321, or a Conexant local sales office. In addition to standard products, customized solutions that take advantage of Conexant's engineering capabilities and high-volume manufacturing resources are also available.
NOTE TO TECHNICAL EDITORS:
Additional Technical information is available upon request
Safe
Harbor Statement
This press release contains statements relating to future results of
Conexant (including certain projections and business trends) that are
"forward-looking statements" as defined in the Private Securities Litigation
Reform Act of 1995. Actual results may differ materially from those
projected as a result of certain risks and uncertainties. These risks
and uncertainties include, but are not limited to: maintaining a consistent
and reliable source of energy; global economic and market conditions,
such as the cyclical nature of the semiconductor industry and the markets
addressed by the company's and its customers' products; demand for and
market acceptance of new and existing products; successful development
of new products; the timing of new product introductions; the availability
and extent of utilization of manufacturing capacity; pricing pressures
and other competitive factors; changes in product mix; fluctuations
in manufacturing yields; product obsolescence; the ability to develop
and implement new technologies and to obtain protection for the related
intellectual property; the successful separation of the Company's Internet
infrastructure and personal networking businesses; the ability to attract
and retain qualified personnel; labor relations of the company, its
customers and suppliers; and the uncertainties of litigation, as well
as other risks and uncertainties, including but not limited to those
detailed from time to time in the company's Securities and Exchange
Commission filings. These forward-looking statements are made only as
of the date hereof, and the company undertakes no obligation to update
or revise the forward-looking statements, whether as a result of new
information, future events or otherwise.
About Conexant Systems, Inc.
Conexant Systems, Inc. is a worldwide leader in semiconductor system
solutions for communications applications. Conexant leverages its expertise
in mixed-signal processing to deliver integrated systems and semiconductor
products through two separate businesses: Conexant and Mindspeed Technologies.
Conexant's personal networking business is focused on digital infotainment,
personal imaging, wireless communications and personal computing products
that are used in mobile communications and the broadband digital home.
Mindspeed Technologies is focused on Internet infrastructure products
including WAN transport, multiservice access and broadband access for
applications that extend from the Internet's access edge all the way
to its optical core. Conexant is headquartered in Newport Beach, Calif.,
and delivered revenues of $2.1 billion for fiscal 2000. The company
is a member of the S&P 500 and NASDAQ-100 Indices. To learn more, visit
us at www.conexant.com.
Other brands and names contained in this release are the property of their respective owners.
# # #