Skyworks and MediaTek Showcase Early 6G FR3 and PC1 RF Front-End Innovations at MWC 2026
At MWC26 Hall 3, Stand 3D10, MediaTek will demonstrate a reference design that uses the SKYR60002 advanced 6G FR3 LNA and power amplifier module with integrated filters designed to support the new 6.425GHz to > 7 GHz spectrum supported in the latest 3GPP standard. The SKYR60002 6G FR3 LNA power amplifier module with integrated filters supports the high linearity, wide bandwidth support, and robust thermal performance needed to comply with stringent 3GPP standard requirements.
In addition,
“6G will introduce a new class of performance requirements, from wider bandwidths and higher frequencies to more advanced air interfaces and system-level efficiency,” said
“Our collaboration with MediaTek is enabling meaningful progress at the front end of next-generation wireless platforms,” said
Availability
Engineering samples of the SKYR60002 6G FR3 6.425GHz to > 7 GHz LNA power amplifier module with integrated filters and the SKY58287-11 UHB PC1 front-end module will be available to early access partners in alignment with MediaTek’s chipset evaluation schedule.
About
Safe Harbor Statement
Any forward-looking statements contained in this media alert are intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. Forward-looking statements include without limitation information relating to future events, results and expectations of
Note to Editors:

Media Relations:Constance Griffiths (949) 230-4867 Constance.Griffiths@skyworksinc.com Investor Relations:Raji Gill (949) 508-0973 Raji.Gill@skyworksinc.com
Source: Skyworks Solutions, Inc.