Skyworks and Xilinx Enable 5G Across Newly Available C-band Spectrum
Companies Demonstrate 280 MHz C-band Solution For 5G Infrastructure
The SKY66523-11 wide instantaneous bandwidth high-efficiency PA has an operational frequency range of 3550 to 4200 MHz and is ideal for use as both a C-band 5G NR small cell PA and as a driver amplifier for Massive MIMO and macro base stations.
The first portion of the C-band spectrum, referred to as “A-block,” is expected to be available by the end of this year. In anticipation of deploying as soon as the A-block spectrum becomes available, OEMs are already in the process of designing C-band systems. B-block and C-block spectrums are expected to be available by the end of 2023.
The demo incorporating the SKY66523-11 PA and the Xilinx Adaptable SoC shows multiple scenarios covering the full 280 MHz C-band spectrum with an occupied bandwidth (OBW) of up to 200 MHz, which is the maximum bandwidth won by any operator during the recent auction. In all scenarios, the combined
“The majority of early 5G deployments are leveraging
“Our demo with
The Xilinx Zynq RFSoC Gen 3 is in full production and contains the direct RF transceivers along with the adaptable CFR (Crest Factor Reduction) and DPD (Digital Pre-Distortion) IP. The SKY66523-11 is part of a 5 × 5 mm pin-to-pin compatible family of PAs supporting major 3GPP bands and is sampling now. To learn more about the SKY66523-11, please visit: https://www.skyworksinc.com/en/Products/Amplifiers/SKY66523-11.
About
Safe Harbor Statement
Any forward-looking statements contained in this press release are intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. Forward-looking statements include without limitation information relating to future events, results and expectations of
Note to Editors:
View source version on businesswire.com: https://www.businesswire.com/news/home/20210623005292/en/
Media Relations:
(949) 231-4207
Investor Relations:
(949) 231-3223
Source: