Skyworks Commences Volume Production of RF Solutions for Broadcom’s 5G WiFi Platforms
The explosion of video consumption and the growing number of wireless devices being used by consumers are putting tremendous stress on existing 802.11 a/b/g/n networks and resulting in video buffering, skipping and battery drain. Broadcom’s new 5G WiFi chips deliver Ethernet-quality speeds three times faster and six times more power efficiently than previous generations of Wi-Fi devices enabling customers to download Web content faster from anywhere in their homes and connect multiple devices to their network simultaneously – all while consuming less device power.
“Consumers want access to high-definition quality video at fast speeds
on multiple devices anywhere in the house — on the TV, or transferred to
tablets and smartphones,” said
“Skyworks is pleased to be partnering with
According to
About Skyworks’ Mobile Connectivity Solutions
- The SKY85803 is a complete 802.11 a/b/g/n/ac wireless local area network (WLAN) RF front-end module (FEM) that provides all the functionality of power amplifiers (PA), filtering, power detector, transmit/receive (T/R) switch, diplexers and associated matching.
- The SE2605L is a high power 802.11bgn WLAN PA module providing the functionality of the PA, power detector, reference voltage generator and input match.
- The SE5003L1-R is a 5 GHz microwave monolithic integrated circuit PA with superior output power, linearity and efficiency.
- The SE5516A is a dual band 802.11a/b/g/n/ac WLAN FEM providing all the functionality of the PAs, filtering, power detector, T/R switch, diplexers and associated matching.
- The SKY13351-378LF and SKY13377-313 are pseudomorphic high electron mobility transistor (pHEMT) gallium arsenide (GaAs) FET integrated/circuit switches.
- The SKY13370-374LF is a GaAs, pHEMT high electron mobility transistor, single pole double throw (SPDT) terminated, high power switch.
- The SKY65404-31 is an ultra low-noise amplifier (LNA) intended for 5 GHz wireless receiver applications.
- The SKY65405-21 is an ultra LNA intended for 2.4 GHz wireless receiver applications.
About Skyworks
Headquartered in
Safe Harbor Statement
This news release includes "forward-looking statements" intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include without limitation information relating to future results and expectations of Skyworks (including without limitation certain projections and business trends). Forward-looking statements can often be identified by words such as "anticipates," "expects," "forecasts," "intends," "believes," "plans," "may," "will," or "continue," and similar expressions and variations or negatives of these words. All such statements are subject to certain risks, uncertainties and other important factors that could cause actual results to differ materially and adversely from those projected, and may affect our future operating results, financial position and cash flows.
These risks, uncertainties and other important factors include, but are
not limited to:uncertainty regarding global economic and financial
market conditions; the susceptibility of the wireless semiconductor
industry and the markets addressed by our, and our customers', products
to economic downturns; the timing, rescheduling or cancellation of
significant customer orders and our ability, as well as the ability of
our customers, to manage inventory; losses or curtailments of purchases
or payments from key customers, or the timing of customer inventory
adjustments; the availability and pricing of third party semiconductor
foundry, assembly and test capacity, raw materials and supplier
components; changes in laws, regulations and/or policies in
These forward-looking statements are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors: Skyworks and
Source:
Skyworks Solutions, Inc.
Media Relations:
Pilar
Barrigas, 949-231-3061
or
Investor Relations:
Stephen
Ferranti, 781-376-3056