Skyworks Delivers World's Most Efficient Front-end Solutions for Internet of Things Applications
Front-end Modules Extend Battery Life and More than
"With consumers and enterprises requiring seamless connectivity, there
is strong market demand for highly integrated, performance-driven analog
solutions delivering significantly improved range and battery life,"
said John O'Neill, vice president of marketing for
In a recent report,
About Skyworks'
The SKY66112-11 is designed for ease of use and maximum flexibility. The multimode front-end module provides an integrated inter-stage matching and harmonic filter, with digital controls compatible with CMOS. The device operates over a wide supply voltage range from 1.2 V to 3.6 V, allowing it to be used in battery-powered applications over a broad spectrum of the battery discharge curve.
Pricing and Availability
The SKY66112-11 is currently available for sampling and production. For
additional information about Skyworks' suite of IoT solutions, please
visit:
About
Safe Harbor Statement
Any forward-looking statements contained in this press release are
intended to qualify for the safe harbor from liability established by
the Private Securities Litigation Reform Act of 1995. Forward-looking
statements include without limitation information relating to future
events, results and expectations of
Note to Editors:
View source version on businesswire.com: http://www.businesswire.com/news/home/20161107006673/en/
Media Relations:
or
Investor Relations:
Source:
News Provided by Acquire Media