Skyworks Enhances Portfolio of Antenna Switch Modules and LTE Switch Solutions
Skyworks’ comprehensive RF switch solutions are based on pHEMT and silicon technology and complement its existing world-class, gallium arsenide and silicon power amplifiers and front-end solutions.
“Skyworks is delighted to once again be offering our customers the
broadest set of switch solutions to meet demanding performance
requirements and design needs,” said
About Skyworks’ Family of Antenna Switch Modules
Skyworks’ ASMs are logic compatible with the world’s leading 3G/4G chipset providers’ interface requirements. In addition to integrated switch and logic, the devices all feature dual low-pass GSM harmonic filters. The ASMs are designed for any combination of 2G/3G multimode cellular applications.
- The SKY13404-466LF is a single pole 10 throw ASM in a compact 2.6 x 3.4 mm quad flat no lead (QFN) package designed for dual and tri mode, high power band switching applications that require low insertion loss. The device features eight high linearity ports providing full flexibility for 2G, 3G and LTE handsets and data cards.
- The SKY13412-487LF is a single pole 12 throw ASM in a 3.0 x 3.8 mm QFN package featuring 10 high linearity ports providing full flexibility for 2G, 3G and LTE handsets and data cards. The device includes port to port RF isolation comparisons in order to optimize signal routing in an increasingly more challenging RF signal environment.
- The SKY18120-11 is a single pole nine throw ASM in an extremely compact 2.5 x 2.5 mm package, 20-pin multi-chip module. The device has three high linearity ports suitable for tri-band 3G/quad-band 2G or TD-SCDMA/2G multi-mode handsets and data cards.
About Skyworks’ LTE Transmit/Receive Switches
Skyworks’ LTE transmit/receive switches are high linearity solutions that can handle multiple input, multiple output receive diversity as well as post power amplifier WCDMA/HSPA+/LTE PA transmit signal routing requirements. Using advanced switching technologies, the devices maintain low insertion loss and high isolation for both transmit and receive switching paths.
- The SKY1341X-485 scalable family of products covers single pole four throw through SP8T switches that allow up to eight bands of WCDMA/LTE transmitting and receiving. The high linearity performance and low insertion loss achieved by the series make in an ideal choice for main/diversity switching commonly used in LTE-based handsets, data cards and tablets that use antenna diversity solutions. The SKY13414-485LF (single pole four throw), SKY13415-485LF (single pole five throw), SKY13416-485LF (single pole six throw), SKY13417-485LF (single pole seven throw) and SKY13418-485LF (SP8T) are a general purpose input/output (GPIO) control logic compatible series of LTE transmit/receive switches in a 2.0 x 2.0 mm lead-frame package.
- The SKY13330-397LF is a SPDT all symmetric port transmit/receive switch in a 2.0 x 2.0 mm lead frame package. Designed for post linear power amplifier single routing to frequency filtering components, this device is differentiated by very low insertion loss and its single bit GPIO control.
Skyworks at
Skyworks will be showcasing its product portfolio in Hall 8, Stand C132
at
About Skyworks
Headquartered in
Safe Harbor Statement
This news release includes “forward-looking statements” intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include without limitation information relating to future results and expectations of Skyworks (including without limitation certain projections and business trends). Forward-looking statements can often be identified by words such as “anticipates,” “expects,” “forecasts,” “intends,” “believes,” “plans,” “may,” “will,” or “continue,” and similar expressions and variations or negatives of these words. All such statements are subject to certain risks, uncertainties and other important factors that could cause actual results to differ materially and adversely from those projected, and may affect our future operating results, financial position and cash flows.
These risks, uncertainties and other important factors include, but are
not limited to: uncertainty regarding global economic and financial
market conditions; the susceptibility of the wireless semiconductor
industry and the markets addressed by our, and our customers', products
to economic downturns; the timing, rescheduling or cancellation of
significant customer orders and our ability, as well as the ability of
our customers, to manage inventory; losses or curtailments of purchases
or payments from key customers, or the timing of customer inventory
adjustments; the availability and pricing of third party semiconductor
foundry, assembly and test capacity, raw materials and supplier
components; changes in laws, regulations and/or policies in
These forward-looking statements are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors: Skyworks and
Source:
Skyworks Media Relations:
Pilar Barrigas, 949-231-3061
or
Skyworks
Investor Relations:
Stephen Ferranti, 781-376-3056