Skyworks Expands Suite of SkyLiTE™ Solutions
Devices Support All Major SoC Platforms and a Growing Number of
The SkyLiTE™ product family incorporates the amplification, switching, Wi-Fi filtering and coupler functionality required to support all major FDD/TDD bands and has been uniquely architected to support the hardware and software compatibility requirements for all major system on a chip platforms. With the addition of external duplexers, this product suite provides OEMs with a scalable and reconfigurable front-end system for broad markets and applications worldwide.
"As the world becomes more connected, OEMs require partners who can
deliver system level solutions across traditional as well as new and
previously unimagined applications," said
According to a
Skyworks' SkyLiTE™ solutions target these fast growing segments.
About Skyworks Expanded Family of SkyLiTE™ Solutions
SKY77643-21 - is a multimode multiband power amplifier module that supports 3G/4G handsets and operates efficiently in WCDMA, TD-SCDMA and LTE modes. The module is fully programmable through a Mobile Industry Processor Interface (MIPI®). The InGaP and silicon die along with the passive components are mounted on a multi-layer laminate substrate and come in a 4.0 x 6.8 x 0.8 mm, 42-pad MCM, SMT package for a highly manufacturable, low cost solution.
SKY77822-21 - is a fully matched, 28-pad surface mount power amplifier module developed for LTE applications. The module includes broadband coverage of FDD LTE Bands 7 and 30, TDD LTE Bands 38/40, and Band 41, all in a compact 4.0 x 3.65 mm package. The device delivers unsurpassed savings in current consumption for data-intensive applications by attaining high efficiencies throughout the entire power range.
SKY77916-21 - is a transmit/receive front-end module that offers the complete transmit VCO-to-antenna and antenna-to-receive SAW filter solution for advanced cellular handsets comprising quad-band GSM, GPRS, EDGE multi-slot operation, and TD-SCDMA and TDD LTE transmission. The FEM fully enables broadband 3G/4G RF switch-through, outward switching of the power amplifier RF inputs, 14 transmit/receive antenna switch ports, and an integrated directional coupler.
SKY77641 - is a multimode multiband power amplifier module that supports 3G/4G handsets and operates efficiently in WCDMA, TD-SCDMA and LTE modes. The module is fully programmable through a MIPI®. The module consists of a WCDMA / LTE block for low, high, and mid-bands, and a multi-function control block with RF input/output ports internally matched to 50 to reduce the number of external components.
About
Headquartered in
Safe Harbor Statement
This news release includes "forward-looking statements" intended to
qualify for the safe harbor from liability established by the Private
Securities Litigation Reform Act of 1995. These forward-looking
statements include without limitation information relating to future
results and expectations of
These risks, uncertainties and other important factors include, but are
not limited to: uncertainty regarding global economic and financial
market conditions; the susceptibility of the semiconductor industry and
the markets addressed by our, and our customers', products to economic
downturns; the timing, rescheduling or cancellation of significant
customer orders and our ability, as well as the ability of our
customers, to manage inventory; losses or curtailments of purchases or
payments from key customers, or the timing of customer inventory
adjustments; the availability and pricing of third-party semiconductor
foundry, assembly and test capacity, raw materials and supplier
components; changes in laws, regulations and/or policies that could
adversely affect either (i) the economy and our customers' demand for
our products or (ii) the financial markets and our ability to raise
capital; our ability to develop, manufacture and market innovative
products in a highly price competitive and rapidly changing
technological environment; economic, social, military and geo-political
conditions in the countries in which we, our customers or our suppliers
operate, including security and health risks, possible disruptions in
transportation networks and fluctuations in foreign currency exchange
rates; fluctuations in our manufacturing yields due to our complex and
specialized manufacturing processes; delays or disruptions in production
due to equipment maintenance, repairs and/or upgrades; our reliance on
several key customers for a large percentage of our sales; fluctuations
in the manufacturing yields of our third-party semiconductor foundries
and other problems or delays in the fabrication, assembly, testing or
delivery of our products; our ability to timely and accurately predict
market requirements and evolving industry standards, and to identify
opportunities in new markets; uncertainties of litigation, including
potential disputes over intellectual property infringement and rights,
as well as payments related to the licensing and/or sale of such rights;
our ability to rapidly develop new products and avoid product
obsolescence; our ability to retain, recruit and hire key executives,
technical personnel and other employees in the positions and numbers,
with the experience and capabilities, and at the compensation levels
needed to implement our business and product plans; lengthy product
development cycles that impact the timing of new product introductions;
unfavorable changes in product mix; the quality of our products and any
remediation costs; shorter-than-expected product life cycles; problems
or delays that we may face in shifting our products to smaller geometry
process technologies and in achieving higher levels of design
integration; and our ability to continue to grow and maintain an
intellectual property portfolio and obtain needed licenses from third
parties, as well as other risks and uncertainties, including, but not
limited to, those detailed from time to time in our filings with the
The forward-looking statements contained in this news release are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors:
View source version on businesswire.com: http://www.businesswire.com/news/home/20160106005439/en/
Media Relations:
or
Investor Relations:
Source:
News Provided by Acquire Media