Skyworks Facilitates Faster Charging for Electric Vehicles
Next-Generation Si89xx Product Family Supports Infrastructure Expansion
This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20230104005027/en/

Skyworks Facilitates Faster Charging for Electric Vehicles With Next-Generation Si89xx Product Family to Support Infrastructure Expansion (Photo: Business Wire)
“Built upon three generations of digital isolation technology, these solutions are engineered to be key enablers in the industry’s shift to vehicle electrification,” said
The steadily growing popularity of EVs amongst consumers has created a market approaching
Skyworks’ new Si89xx products provide accurate, precise measurement readings of the current and voltage involved in the operation of power control systems, including 75 kV/µs immunity to fast transients and accuracy over temperature. This minimizes loss of power and inherently makes the system more efficient, allowing for charging devices to more swiftly transfer power. This increased functionality enables charging improvements for the EV industry and industrial applications across different markets, including wireless infrastructure, data centers and wired communications. As the telecommunications industry shifts toward standalone 5G networks and fixed wireless access, there is an increased emphasis placed on the importance of power management. Accurate current and voltage measurement in telecom power supply equipment results in increased efficiency and allows for detailed monitoring, resulting in reduced cost, less downtime and improved system management.
Additional Product Information:
Samples of the Si8921, Si893x and Si894x devices are available now. Skyworks’ Si89xx family consists of the Si8921 isolated analog amplifiers, the Si893x isolated voltage sensors and the Si8941/6/7 isolated DSM devices. These devices are optimized for voltage or shunt-current sensing and provide typical offset error as low as ±40 µV and ±0.1% gain error. Additionally, offering a typical offset drift as low as ±0.5 µV/˚C and typical gain drift as low as –4 ppm/˚C, allows for exceptional accuracy across temperature. As a result of these benefits, The Si89xx devices can offer one of the industry’s highest signal-to-noise ratios (SNR)—up to 90 dB.
The Si89xx family offers a solution optimized to meet the challenges of measurement in high-voltage systems, providing low drift accuracy, low signal delay and transient noise immunity. These expanded devices will enhance design flexibility with the following options:
- Current or voltage-optimized devices with single-ended, differential or DSM output
- ±62.5 mV, ±250 mV or 2.5 V input ranges
- A stretched wide-body SOIC-8 package to support 5 kVrms isolation and 8 mm creepage/clearance and a compact narrow-body SOIC-8 to support 2.5 kVrms isolation
About
Safe Harbor Statement
Any forward-looking statements contained in this press release are intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. Forward-looking statements include without limitation information relating to future events, results and expectations of
Note to Editors:
1 Electric Vehicles Worldwide, Statista,
View source version on businesswire.com: https://www.businesswire.com/news/home/20230104005027/en/
Media Relations:
(949) 231-4207
Investor Relations:
(949) 231-3223
Source: