Skyworks Front End Solutions Support Broadcom 5G WiFi Platforms
Enable Industry's Fastest Download Speeds
"With digital content consumption on the rise, particularly as consumers
watch video on more devices and in more places around the home, Broadcom
is closely collaborating with
"Skyworks is excited to be a part of Broadcom's 5G WiFi platforms
enabling next generation mobile devices and customer premise equipment,"
said
By next year, 802.11ac is expected to be the dominant standard and its reach is expected to go well beyond just smartphones, tablets and computers. According to a study by Strategy Analytics, sales of consumer devices compatible with 802.11ac, including routers and gateways, will grow and surpass one billion units by the end of 2015 and 2.8 billion in 2017. The 802.11ac deployment will initially involve smartphones and tablets with connected televisions, media players and other devices to follow.
About Broadcom's 5G WiFi Solutions
By creating more reliable whole-home coverage, Broadcom's 5G WiFi technology overcomes the digital content and wireless device challenge. Broadcom's family of 5G WiFi solutions dramatically improves the wireless range in the home, allowing consumers to watch HD-quality video from more devices, in more places, simultaneously. The increased speed enables consumers to download web content from a mobile device faster and quickly synch large files, such as videos, in a fraction of the time. Visit www.broadcom.com to learn more.
About Skyworks' Mobile Connectivity Solutions
Designed to meet stringent linearity conditions of 802.11ac standard, the SE5516A delivers < 2 percent error vector magnitude at rated AC power. All RF ports are matched to 50 Ω to simplify printed circuit board layout and the interface to the transceiver RFIC. The device also includes a transmitter power detector with 20 dB of dynamic range for each transmit chain. Each power amplifier (PA) has a separate digital enable control for transmitter on/off control. The power ramp rise/fall time is less than 0.4 µsec. It also provides a notch filter from 3.260 — 3.267 GHz prior to the input of each 2.4 GHz and 5 GHz PAs, respectively. The solution is housed in a 4 x 4 x 1 millimeter (mm), halogen and lead free, restriction of hazardous substances compliant, moisture sensitivity level, 3 land grid array package.
The SKY85302-11 is a complete 802.11ac WLAN RF FEM with a Bluetooth® port. The device provides all of the functionality of a fully matched PA, power detector, harmonic filter, low-noise amplifier (LNA) and single-pole, triple-throw switch. The FEM also provides a complete 2.4 GHz solution from the output of the transceiver to the antenna, and from the antenna to the input of the transceiver. The LNA increases the receive sensitivity of embedded solutions to improve range or to overcome the insertion loss of cellular filters, often included for mobile applications. In addition, the device includes a transmitter power detector with 20 dB of dynamic range, and a digital-enable control for transmitter power ramp on/off control. The FEM is also provided in an ultra-compact, 16-pin, 2.5 x 2.5 mm, quad-flat, no-lead (QFN) package.
The SKY85706-11 is a highly integrated, 5 GHz FEM incorporating a single-pole, double throw T/R switch, an LNA with bypass, and a PA intended for mobile/portable, 802.11n/ac applications and systems. An enable/disable function is included, allowing power savings during off mode. In addition, an integrated power detector with 20 dB of dynamic range is included to provide closed-loop power control within the system. The FEM is also provided in a compact, 16-pin, 2.5 x 2.5 QFN package.
About
Headquartered in
Safe Harbor Statement
This news release includes "forward-looking statements" intended to
qualify for the safe harbor from liability established by the Private
Securities Litigation Reform Act of 1995. These forward-looking
statements include without limitation information relating to future
results and expectations of
These risks, uncertainties and other important factors include, but are
not limited to: uncertainty regarding global economic and financial
market conditions; the susceptibility of the semiconductor industry and
the markets addressed by our, and our customers', products to economic
downturns; the timing, rescheduling or cancellation of significant
customer orders and our ability, as well as the ability of our
customers, to manage inventory; losses or curtailments of purchases or
payments from key customers, or the timing of customer inventory
adjustments; the availability and pricing of third party semiconductor
foundry, assembly and test capacity, raw materials and supplier
components; changes in laws, regulations and/or policies, including the
possibility of expiring tax cuts combined with mandatory reductions in
federal spending, in
The forward-looking statements contained in this news release are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors:
Skyworks Media Relations:
or
Source:
News Provided by Acquire Media