Skyworks Introduces the Most Comprehensive Portfolio of LTE Power Amplifiers and Front-End Modules
This multi-band and multi-mode family of products, which now includes
two new PA modules and four new FEMs, supports 13 frequency bands - - -
the largest across the industry - - - and provides the most complete and
flexible set of options for manufacturers developing and building
4G-enabled handsets, infrastructure basestations, wireless PC cards, and
a variety of other embedded solutions. The portfolio includes the
industry’s first PA modules supporting LTE-FDD for
“Skyworks’ newest product offerings solidify the company’s 4G leadership
position and illustrate our commitment to providing the smallest, most
cost-effective and highest performance wireless analog solutions,” said
Dr.
About Skyworks’ Newest LTE Power Amplifiers and Front-End Modules
The SKY77455, SKY77456, SKY77457 and SKY77458 -- compact front-end modules that support Bands I, IV/X, V/VI and VIII, respectively -- are fully matched and completely compliant for LTE, as well as HSDPA and WCDMA standards. These FEMs integrate the PA, interstage filter, input/output matching, power detection, and duplexer functionality in a small 4 x 7 millimeter (mm) form factor.
The SKY77449 for Bands XIII and XIV, and the SKY77453 for Bands XII and XVII, are both fully matched PA modules developed for 4G LTE/EUTRAN standards. They integrate all active RF circuitry, including the input, interstage and output matching circuits and power detector functionality within a single 4 x 4 x 0.85 mm low-profile package.
Using Skyworks' advanced indium gallium phosphide (InGaP) bipolar field effect transistor (BiFET) design, which provides advanced bias and detection architecture implementation, and Skyworks GreenTM packaging solutions, the family also supports low-operating voltage down to 3 volts (V) with high power added efficiency (PAE), high reliability and quality. The portfolio also delivers high linear power under quadrature phase-shift keying (QPSK), 16 quadrature amplitude modulations (QAM), and wideband code division multiple access (WCDMA) modulation, with up to 20 megahertz (MHz) in bandwidth and partial or full resource block allocation.
The SKY77445 PA module for Band VII and the SKY77441 FEM for Bands 38 and 40 were introduced in 2008 and complete this newly expanded LTE product family.
Pricing and Availability
Samples of all new devices are currently available, with volume production scheduled to begin this year. For customized pricing, please contact sales@skyworksinc.com.
Skyworks at
Skyworks will be showcasing its portfolio of Intera™ solutions in Hall
8, Stand C132 at
About Skyworks
Headquartered in
Safe Harbor Statement
This news release includes "forward-looking statements" intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include information relating to future results and expectations of Skyworks (including certain projections and business trends). Forward-looking statements can often be identified by words such as "anticipates," "expects," "forecasts," "intends," "believes," "plans," "may," "will," "continue," similar expressions, and variations or negatives of these words. All such statements are subject to certain risks and uncertainties that could cause actual results to differ materially and adversely from those projected, and may affect our future operating results, financial position and cash flows.
These risks and uncertainties include, but are not limited to:
unprecedented uncertainty regarding global economic and financial market
conditions; the susceptibility of the wireless semiconductor industry
and the markets addressed by our, and our customers', products to
economic downturns; the timing, rescheduling or cancellation of
significant customer orders and our ability, as well as the ability of
our customers, to manage inventory; losses or curtailments of purchases
or payments from key customers, or the timing of customer inventory
adjustments; changes in laws, regulations and/or policies in
These forward-looking statements are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors: Skyworks,
Source:
Skyworks Media Relations:
Amanda Ingalls
949-231-3045
or
Skyworks
Investor Relations:
Thomas Schiller
949-231-4700