sub-page-banner

Press Release

Skyworks Introduces New Programmable Bulk Acoustic Wave Clocks for 5G, 6G, and Data Center Applications

Breakthrough Timing Solutions Deliver Ultra-Low Jitter for 224G PAM4 SerDes and Class C/D Compliance for IEEE 1588 Synchronization

IRVINE, Calif., Nov. 06, 2025 (GLOBE NEWSWIRE) -- Skyworks Solutions, Inc. (Nasdaq: SWKS), an innovator of high-performance analog and mixed-signal semiconductors connecting people, places and things, today announced a new family of ultra-low jitter programmable clocks designed to meet the increasing demands of next-gen connectivity. The SKY63101/02/03 Jitter Attenuating Clocks and SKY69001/02/101 NetSync™ Clocks leverage Skyworks’ proven DSPLL® and MultiSynth™ timing architecture and Skyworks’ advanced Bulk Acoustic Wave (BAW) technology to deliver breakthrough performance in low-jitter timing applications.

Together these new clocks redefine the benchmark for wireline, wireless, and data center timing solutions. The SKY63101/02/03 clocks provide industry-leading Synchronous Ethernet clock jitter of just 17 femtoseconds for 224G PAM4 SerDes, making them suitable for wireline and data center applications such as 800G/1.2T/1.6T optical networking and Data Center Interconnect (DCI) optical links. 

The SKY69001/02/101 clocks deliver best-in-class CPRI clock phase noise of -142 dBc/Hz at 100 kHz offset and support for IEEE 1588 Class C/D synchronization leveraging Skyworks AccuTime™ 1588 software, making them well-suited for wireless applications such as 5G and next-generation 6G massive MIMO radios. 

“Skyworks is committed to being an innovation leader in the timing industry,” said James Wilson, vice president and general manager at Skyworks. “By combining our advanced BAW technology with industry-leading DSPLL and MultiSynth timing architectures, these devices represent a significant leap forward in performance, reliability and integration. We are excited to bring these groundbreaking products to the market and support the evolving needs of 5G/6G networks, wireline and data center communications.” 

Skyworks is a recognized leader in BAW technology, known for manufacturing high-volume BAW GHz filters across consumer, IoT and infrastructure applications. Skyworks’ expertise in BAW technology has been instrumental in advancing 5G and Wi-Fi radio front-end solutions, leveraging silicon-based fabrication processes to ensure high performance and reliability in these critical applications.

At the heart of every Skyworks BAW filter is a multi-GHz, high Q-factor, low phase noise BAW micro-resonator. Skyworks’ newest timing products leverage this BAW frequency reference to eliminate the need for external quartz crystal, XO and VCXO references, minimizing bill of materials (BOM) count and complexity while improving clock jitter and overall system reliability.

The SKY69001/02/101 and SKY63101/02/02 family of products feature exceptional multi-channel noise isolation and on-chip power supply noise rejection, enabling a single device to generate multiple, non-related frequencies without compromising jitter, phase noise and spurious performance.

The SKY69001/02/101 and SKY63101/02/02 products share a common footprint and application programming interface (API), making it easy for designers to transition between using a jitter attenuating clock and a network synchronizer depending on system-level timing requirements. The SKY63101/02/03 and SKY69001/02/101 clocks are factory and field-programmable using integrated flash memory, enabling the devices to boot up with a preconfigured frequency plan and support easy in-field reconfigurability. These features enable system designers to develop a single hardware solution and tailor the solution for each application fully in software.

The SKY69001/02/101 and SKY63101/02/02 family of products have also been optimized to work in challenging environmental conditions. All these new devices support a -40 to +95°C ambient temperature range, making them ideal for non-temperature-controlled applications like wireless base stations. Typical power consumption is 1.2W, more than 60% lower than traditional solutions.

Key Features

SKY63101/02/03 Jitter Attenuating Clocks

  • Eliminates quartz crystal or XO in optical, Ethernet and data center applications
  • 1, 2, or 3 DSPLLs
  • 0, 1, or 2 MultiSynth fractional dividers
  • Any-frequency clock generation: 8kHz to 3.2GHz
  • 5 differential clock inputs and 16 differential clock outputs
  • LVDS, HCSL, LVPECL, LVCMOS, S-LVDS, and CML
  • Integrated flash memory and BAW resonator

     

SKY69001/02/101 Wireless NetSync™ Clocks

  • Eliminates XO or VCXO in wireless CPRI applications
  • 1, 2, or 3 DSPLLs
  • 0, 1, or 2 MultiSynth fractional dividers
  • Any-frequency clock generation: PP2S to 3.2 GHz
  • 5 differential clock inputs and 16 differential clock outputs
  • IEEE 1588 network synchronization with Class C/D compliance
  • JESD204B/C support
  • LVDS, HCSL, LVPECL, LVCMOS, S-LVDS, and CML
  • Integrated flash memory and BAW resonator

     

Availability

Samples and production quantities of the SKY69001/02, SKY69101, and SKY63101/02/03 are available now. Evaluation is supported via the SKY63103-EVB development kit and the SKY69101-EVB development kit.

For more information, please visit skyworksinc.com/Products/Timing.

About Skyworks

Skyworks Solutions, Inc. is empowering the wireless networking revolution. We are a leading developer, manufacturer and provider of analog and mixed-signal semiconductors and solutions for numerous applications, including aerospace, automotive, broadband, cellular infrastructure, connected home, defense, entertainment and gaming, industrial, medical, smartphone, tablet and wearables.

Skyworks is a global company with engineering, marketing, operations, sales and support facilities located throughout Asia, Europe and North America and is a member of the S&P 500® market index (Nasdaq: SWKS). For more information, please visit Skyworks’ website at: www.skyworksinc.com.

Safe Harbor Statement

Any forward-looking statements contained in this media alert are intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. Forward-looking statements include without limitation information relating to future events, results and expectations of Skyworks. Forward-looking statements can often be identified by words such as “anticipates,” “expects,” “forecasts,” “intends,” “believes,” “plans,” “may,” “will” or “continue,” and similar expressions and variations or negatives of these words. Actual events and/or results may differ materially and adversely from such forward-looking statements as a result of certain risks and uncertainties including, but not limited to, our ability to timely and accurately predict market requirements and evolving industry standards and to identify opportunities in new markets; our ability to develop, manufacture, and market innovative products and avoid product obsolescence; our ability to compete in the marketplace and achieve market acceptance of our products; the level of widespread deployment or adoption of commercial 5G networks, AI and other new technologies; the availability and pricing of third-party semiconductor foundry, assembly and test capacity, raw materials and supplier components; the quality of our products; our products’ ability to perform under stringent operating conditions; and other risks and uncertainties identified in the “Risk Factors” section of Skyworks' most recent Annual Report on Form 10-K (and/or Quarterly Report on Form 10-Q) as filed with the Securities and Exchange Commission (“SEC”). Copies of Skyworks' SEC filings can be obtained, free of charge, on Skyworks' website (www.skyworksinc.com) or at the SEC's website (www.sec.gov). Any forward-looking statements contained in this media alert are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.

Note to Editors: Skyworks, the Skyworks symbol, NetSync, DSPLL, and MultiSynth are trademarks or registered trademarks of Skyworks Solutions, Inc., or its subsidiaries in the United States and other countries. Third-party brands and names are for identification purposes only and are the property of their respective owners.

Media Relations:
Constance Griffiths
(949) 230-4867
Constance.Griffiths@skyworksinc.com
Investor Relations:
Raji Gill
(949) 508-0973
Raji.Gill@skyworksinc.com
  

 


Primary Logo

Source: Skyworks Solutions, Inc.