Skyworks Introduces PA Plus, A Highly Efficient Wireless LAN Power Amplifier With On-Chip Filtering
Solution to Become An Integral Part of Skyworks' 802.11b/g WLAN Front-End Module Family
-- Editor's Note: Skyworks will be demonstrating its innovative wireless semiconductor solutions at the MTT-S trade show, June 8-10, 2004, in Fort Worth, Texas at the Fort Worth Convention Center in booth #1037.
Skyworks Solutions, Inc. (Nasdaq:SWKS), the industry's leading wireless semiconductor company focused on radio frequency (RF) and complete cellular system solutions for mobile communications applications, today announced the launch of yet another highly innovative, high-performance power amplifier (PA) - this time for 802.11 b/g WLAN systems.
Leveraging its leadership positions in PA modules for cellular applications, Skyworks' new PA Plus with on-chip harmonic filtering, eliminates the need for additional filtering in the transmit chain. The PA delivers superior output power at high data rates, improving WLAN throughput while extending battery life in handheld device applications such as PCMCIA cards, mini PCI cards, access points and other wireless data designs. Additionally, PA Plus offers outstanding linearity and efficiency with its streamlined applications circuit, reducing the component count by 30 percent when compared to alternative PA solutions, and cutting the size and cost of WLAN products while simplifying board layout.
"Skyworks' new PA Plus solution builds on the company's leadership position in highly efficient PA modules for cellular applications," said Mark Comerford, director of wireless data at Skyworks. "With PA Plus, designers will be able to eliminate some costly filters and other components in order to realize a significant bill of materials reduction. Initially available as a discrete product, the PA will become an integral part of Skyworks' next generation WLAN front-end modules, taking advantage of our broad product and process technology portfolio."
In 2003, Skyworks introduced the world's first 802.11a/b/g front-end modules, demonstrating its cellular handset RF integration expertise in combining PA, switch and filter functions into a single convenient module that dramatically reduced system design time and cost. Since then, Skyworks has expanded its family to support virtually any combination of 802.11 features and capabilities, including several frequency bands and multiple modulation techniques. Customers can develop complete architectures with fewer components than with alternative solutions, saving valuable space across all wireless data platforms.
About the PA Plus ( SKY65006)
Skyworks' PA Plus is a highly efficient WLAN power amplifier for 802.11 b/g applications. A key feature of the PA is its versatility to be biased at higher voltage levels to deliver an additional 15 percent of output power for improved performance in access point and higher-voltage USB designs. The PA delivers 17 dBm of linear output power for 802.11g and 20 dBm of linear output power for 802.11b, while consuming a low 100 mA and 120 mA of power, respectively, when operating from a 3.3-volt supply. At a VCC of 5.0 volts, designers can achieve up to 3 dBm of additional output power from the PA, for access point and USB applications. It is internally matched to 50 Ohms at both the input and the output and includes a temperature compensated output power detector. A version with an integrated directional power detector will also be available by the end of 2004. On-chip harmonic filtering further eliminates the need for additional filtering in the transmit chain for wireless applications where low current consumption is critical.
PA Plus is manufactured using the company's indium gallium arsenide (InGaP) heterojunction bipolar transistor (HBT) process to deliver optimum performance and reliability. It is available in a 3 x 3mm low-cost, quad flat no-lead (QFN) package. Pricing is $0.55 each in volumes of 100,000. Volume production will commence this quarter.
About Skyworks
Skyworks Solutions, Inc. is the industry's leading wireless semiconductor company focused on RF and complete cellular system solutions for mobile communications applications. The company provides front-end modules, RF subsystems and cellular systems to handset, WLAN and infrastructure customers.
Skyworks is headquartered in Woburn, Mass., with executive offices in Irvine, Calif. The company has design, engineering, manufacturing, marketing, sales and service facilities throughout North America, Europe, Japan, China, Korea, Taiwan and India. For more information please visit www.skyworksinc.com.
Safe Harbor Statement
This news release includes "forward-looking statements" intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include information relating to future results of Skyworks (including certain projections and business trends). Forward-looking statements can often be identified by words such as "anticipates," "expects," "intends," "believes," "plans," "may," "will," "continue," similar expressions, and variations or negatives of these words. All such statements are subject to certain risks and uncertainties that could cause actual results to differ materially and adversely from those projected, and may affect our future operating results, financial position and cash flows.
These risks and uncertainties include, but are not limited to: global economic and market conditions, such as the cyclical nature of the semiconductor industry and the markets addressed by the company's and its customers' products; demand for and market acceptance of new and existing products; the ability to develop, manufacture and market innovative products in a rapidly changing technological environment; the ability to compete with products and prices in an intensely competitive industry; product obsolescence; losses or curtailments of purchases from key customers or the timing of customer inventory adjustments; the timing of new product introductions; the availability and extent of utilization of raw materials, critical manufacturing equipment and manufacturing capacity; pricing pressures and other competitive factors; changes in product mix; fluctuations in manufacturing yields; the ability to continue to grow and maintain an intellectual property portfolio and obtain needed licenses from third parties; the ability to attract and retain qualified personnel; labor relations of the company, its customers and suppliers; economic, social and political conditions in the countries in which Skyworks, its customers or its suppliers operate, including health and security risks, possible disruptions in transportation networks and fluctuations in foreign currency exchange rates; and the uncertainties of litigation, as well as other risks and uncertainties, including but not limited to those detailed from time to time in the company's Securities and Exchange Commission filings.
These forward-looking statements are made only as of the date hereof, and the company undertakes no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Skyworks and PA Plus are trademarks or registered trademark of Skyworks Solutions, Inc. or its subsidiaries in the U.S. and in other countries. All other brands and names listed are trademarks of their respective companies.
CONTACT:
Skyworks Media Relations
Lisa Briggs, 949-231-4553
lisa.briggs@skyworksinc.com
or
Skyworks Investor Relations
Thomas Schiller, 949-231-4700
SOURCE: Skyworks Solutions, Inc.