Skyworks Launches Family of Solutions for Rapidly Growing Small Cell Market
Devices Enable Faster Data Rates Across Diverse Environments; Global Operators Utilizing in Network Platforms
This Smart News Release features multimedia. View the full release here: http://www.businesswire.com/news/home/20170227006763/en/
(Photo: Business Wire)
"By utilizing Skyworks' highly efficient solutions, SpiderCloud has
further enhanced its market-proven LTE small cell network platforms,
giving mobile operators the ability to deliver unprecedented cellular
coverage, capacity and smart applications to enterprises and other
customers," said
"With the addition of these small cell solutions,
According to a recent MarketandMarkets research report, increasing
demand for higher bandwidth spectrum, rising mobile data traffic on
present networks, and telecom-based technological growth, are all
boosting the demand for small cell networks. The increasing usage of
smartphones and data services by consumers has resulted in huge data
traffic over the current networks, leading to network congestion and
dropped calls. Small cells can offload data from licensed
spectrum/unlicensed spectrum by using the combination of technologies
such as 2G, 3G, and LTE along with carrier grade Wi-Fi. As a result,
MarketsandMarkets expects the global small cell networks market to grow
from
About Skyworks' Solutions for Enterprise Small Cell Applications
The SKY6629x high-efficiency, four watt power amplifiers consists of the following:
SKY66299 - 1900 to 2000 MHz
SKY66297 - 2490 to 2690 MHz
SKY66296 - 700 to 800 MHz
SKY66295 - 800 to 900 MHz
SKY66294 - 2000 to 2300 MHz
SKY66293 - 3400 to 3800 MHz
SKY66292 - 2300 to 2400 MHz
SKY66291 - 1805 to 1880 MHz
For more information about Skyworks' solutions for small cell, please contact: sales@skyworksinc.com or visit our Small Cell web page. The SKY6629x family is currently in production.
About
About
Safe Harbor Statement
Any forward-looking statements contained in this press release are
intended to qualify for the safe harbor from liability established by
the Private Securities Litigation Reform Act of 1995. Forward-looking
statements include without limitation information relating to future
events, results and expectations of
Note to Editors:
View source version on businesswire.com: http://www.businesswire.com/news/home/20170227006763/en/
Media Relations:
or
Investor Relations:
Source:
News Provided by Acquire Media