Skyworks Unveils Family of Front-End Modules with Breakthrough Power Control Performance for Quad Band Cellular Handsets
“Skyworks’ highly integrated front-end modules utilize a small footprint
and unique power control scheme to improve total radiated power
performance – a key factor in today’s advanced handsets,” said
Skyworks’ 2.5G and 3G FEMs with Unique Power Control Scheme
The SKY77527 (8 x 6 x 1.12 mm) – optimized for Infineon’s reference designs – and the SKY77528 (8 x 6 x 1.1 mm) – supporting Broadcom’s platform – consist of a GSM850/900 and DCS1800/PCS1900 PA block, impedance matching circuitry for 50 ohm input and output impedances, a multifunction PA control (MFC) block, low pass harmonic rejection filters, and a single pole six throw (SP6T) antenna transmit/receive (T/R) switch. The MFC in the SKY77527 provides “pinout” for interoperation with an external power control loop. The external circuit uses the linear detector output to provide closed loop power control in EDGE and gaussian minimum shift keying (GMSK) modes of operation.
With an integrated saturation, detection and correction circuit, the SKY77528 also improves phone reliability with output radio frequency spectrum (ORFS) performance in voltage standing wave radio (VSWR) and low-battery condition.
The SKY77529 (7.5 x 7 x 1.1 mm) – optimized for Infineon’s reference designs – consists of a GSM850/900 PA block and a DCS1800/PCS1900 PA block, a printed directional coupler for each block impedance-matching circuitry for 50 ohm input and output impedances, a MFC block, low pass harmonic rejection filters, and a SP8T antenna T/R switch. The FEM, with an antenna that connects to any one of two reception (Rx) or four wideband code division multiple access (WCDMA) Rx/Tx ports, incorporates full support for a serial peripheral interface (SPI) bus function.
The SPI controller, which offers convenient digital control, accepts SPI telegrams with data fields that support PA and switchplexer-related functions. All FEM operating modes and switch states shall be determined by the SPI telegram. The MFC provides pinout for interoperation with a specified transceiver that will establish a closed loop power control mechanism. The external circuit uses the linear detector output to set a fixed bias point for 8PSK (EDGE) mode and a variable bias point for GMSK (GSM) mode, which allows easy-to-implement timing and calibration.
Finally, the SKY77546 (7 x 6 x 1.0 mm) consists of an extended global system for mobile communications (EGSM900) PA block and a DCS1800 PA block, impedance-matching circuitry for 50 ohm inputs and outputs, a multi-function PA control block, low pass harmonic rejection filter, and a Tx/Rx antenna switch. Supporting MediaTek’s low-cost EDGE platform, the module contains a diplexer filter which provides excellent harmonics and electrostatic discharge (ESD) performance.
Pricing and Availability
For customized pricing, please contact sales@skyworksinc.com. Availability is as follows:
- The SKY77527 – In volume production.
- The SKY77528 – In volume production.
- The SKY77529 – Sampling now.
- The SKY77546 – Sampling Q2 2009.
About Skyworks
Headquartered in
Safe Harbor Statement
This news release includes "forward-looking statements" intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include information relating to future results and expectations of Skyworks (including certain projections and business trends). Forward-looking statements can often be identified by words such as "anticipates," "expects," "forecasts," "intends," "believes," "plans," "may," "will," "continue," similar expressions, and variations or negatives of these words. All such statements are subject to certain risks and uncertainties that could cause actual results to differ materially and adversely from those projected, and may affect our future operating results, financial position and cash flows.
These risks and uncertainties include, but are not limited to:
unprecedented uncertainty regarding global economic and financial market
conditions; the susceptibility of the wireless semiconductor industry
and the markets addressed by our, and our customers', products to
economic downturns; the timing, rescheduling or cancellation of
significant customer orders and our ability, as well as the ability of
our customers, to manage inventory; losses or curtailments of purchases
or payments from key customers, or the timing of customer inventory
adjustments; changes in laws, regulations and/or policies in
These forward-looking statements are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors: Skyworks,
Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=5916482&lang=en
Source:
Skyworks Media Relations:
Amanda Ingalls, 949-231-3045
or
Skyworks
Investor Relations:
Thomas Schiller, 949-231-4700