Skyworks Unveils Family of Front-End Solutions with the Industry’s Best-in-Class Power Added Efficiency
“Today’s applications and devices require improved efficiency at high
power,” said
According to Ericsson, a world-leading provider of telecommunications equipment and services, mobile broadband connections, which provide the means to connect to the Internet and download data or other content, are exploding. They estimate that there were more than 500 million mobile broadband subscribers globally in 2010 with subscriptions expected to grow to more than 2.5 billion subscribers in 2014, representing a compounded annual growth rate of 44 percent.
About Skyworks’ SkyHi™ Front-end Solutions
- The SKY77619 (Bands I, II, III, IV, V and VIII) is a multimode, multiband power amplifier module (PAM) that supports 2.5G/3G and 4G handsets and operate efficiently in GSM, EGPRS, EDGE, WCDMA and LTE modes.
- The SKY77733 (Bands XIII/XIV) and SKY77737 (Bands XII/XVII) are fully matched surface mount modules PAMs developed for LTE applications.
- The SKY77751 and SKY77752 are dual band power amplifiers supporting either Bands I and VIII or II and V. They come in a 3 x 4 mm package and have either a single RF input or dual RF input for CDMA and WCDMA applications.
- The SKY77761 is a PAM that is a fully matched 10-pad surface mount module developed for WCDMA applications.
- The SKY77762, SKY77764, SKY77765 and SKY77768 are PAMs supporting Band I, II, IV, V and VIII, respectively, developed for CDMA, WCDMA and LTE applications.
Skyworks at
Skyworks will be showcasing its product portfolio in Hall 8, Stand C132
at
About Skyworks
Headquartered in
Safe Harbor Statement
This news release includes "forward-looking statements" intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include without limitation information relating to future results and expectations of Skyworks (including without limitation certain projections and business trends). Forward-looking statements can often be identified by words such as "anticipates," "expects," "forecasts," "intends," "believes," "plans," "may," "will," or "continue," and similar expressions and variations or negatives of these words. All such statements are subject to certain risks, uncertainties and other important factors that could cause actual results to differ materially and adversely from those projected, and may affect our future operating results, financial position and cash flows.
These risks, uncertainties and other important factors include, but are
not limited to: uncertainty regarding global economic and financial
market conditions; the susceptibility of the wireless semiconductor
industry and the markets addressed by our, and our customers', products
to economic downturns; the timing, rescheduling or cancellation of
significant customer orders and our ability, as well as the ability of
our customers, to manage inventory; losses or curtailments of purchases
or payments from key customers, or the timing of customer inventory
adjustments; the availability and pricing of third party semiconductor
foundry, assembly and test capacity, raw materials and supplier
components; changes in laws, regulations and/or policies in
These forward-looking statements are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors: Skyworks and
Source:
Skyworks Media Relations:
Pilar Barrigas, 949-231-3061
or
Skyworks
Investor Relations:
Stephen Ferranti, 781-376-3056