Skyworks Unveils Family of High Power Control Devices for Diverse Market Applications
“Skyworks is delighted to be offering customers unique and innovative
products for their demanding RF design needs,” said
About Skyworks’ New High Power SPDT Switches
The SKY12207-478LF (0.9 – 4.0 GHz), SKY12208-306LF (0.02 – 2.7 GHz) and SKY12210-478LF (0.9 – 4.0 GHz) are high power SPDT silicon-based PIN diode switches. The 4 x 4 millimeter, 16-pin quad flat no lead packaged devices features low insertion loss (0.4dB), high isolation (44 dB), excellent power handling (50 and 100 Watts) and superb linearity with low direct current (DC) power consumption. They all operate with a 5 or 28 V positive DC voltage supply across a broad frequency range (20 MHz – 4.0 GHz). Skyworks has also developed a complementary driver application circuit to align with these switches.
Pricing and Availability
Skyworks’ new switches are currently available. For volume pricing, samples, evaluation boards and integrated driver circuit, please contact sales@skyworksinc.com.
Skyworks at IEEE MTT-S 2012
Skyworks will be exhibiting its products in booth #1507 at MTT-S 2012,
being held
About Skyworks
Headquartered in
Safe Harbor Statement
This news release includes “forward-looking statements” intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include without limitation information relating to future results and expectations of Skyworks (including without limitation certain projections and business trends). Forward-looking statements can often be identified by words such as “anticipates,” “expects,” “forecasts,” “intends,” “believes,” “plans,” “may,” “will,” or “continue,” and similar expressions and variations or negatives of these words. All such statements are subject to certain risks, uncertainties and other important factors that could cause actual results to differ materially and adversely from those projected, and may affect our future operating results, financial position and cash flows.
These risks, uncertainties and other important factors include, but are
not limited to: uncertainty regarding global economic and financial
market conditions; the susceptibility of the wireless semiconductor
industry and the markets addressed by our, and our customers’, products
to economic downturns; the timing, rescheduling or cancellation of
significant customer orders and our ability, as well as the ability of
our customers, to manage inventory; losses or curtailments of purchases
or payments from key customers, or the timing of customer inventory
adjustments; the availability and pricing of third party semiconductor
foundry, assembly and test capacity, raw materials and supplier
components; changes in laws, regulations and/or policies in
These forward-looking statements are made only as of the date hereof, and we undertake no obligation to update or revise the forward-looking statements, whether as a result of new information, future events or otherwise.
Note to Editors: Skyworks and
Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=50313064x&lang=en
Source:
Skyworks Solutions, Inc.
Media Relations:
Pilar
Barrigas, 949-231-3061
Investor Relations:
Stephen
Ferranti, 781-376-3056